Oct 6, 2020

Double sheet detection made simple: two ultrasonic sensors, three sizes, various object materials
Teaserbilder_News_Baumer_Double-sheet-detection-made-simple-with-ultrasonic-sensors_ML_20200921_PH_600x338.jpg
Increased process safety thanks to reliable detection of one or more layers even with critical material thicknesses.
Two product families, many possible solutions: The high-performance ultrasonic sensors U300 and U500/ UR18 from Baumer offer a multitude of integrated functions and adjustment options. These allow the sensor to be optimally adjusted to the application. A new double sheet detection function has now been implemented in the through beam sensor of these series.

Double sheet detection: Reliable detection of one or more layers 

Double sheets often cause machine downtime and resulting repair costs if necessary. This is prevented by the reliable detection of double sheets with the U300 and U500/UR18 product families of ultrasonic through beam sensors. This increases process safety and prevents damage and waste in further process steps. The receiver of the through beam sensor is equipped with two binary switching outputs as well as an IO-Link interface. The sensor reliably detects the most common materials in the standard setting. If critical material thicknesses occur, the sensor can be optimally taught in for this through parameter configuration. Both in IO-Link mode and in switching mode, the sensor detects one, two, or more layers of materials such as foil, paper, cardboard, labels, or even thin metal sheets.

Typical applications in addition to double sheet detection are film tear detection, bonding surface detection, and label inspection. Here one encounters very diverse materials and their thickness as well as extremely varied installation conditions. This is no problem for the ultrasonic sensors from Baumer. The through beam sensor can be flexibly adjusted to materials and the installation situation, such as the distance. Via IO-Link, the parameters can be easily and quickly adjusted to critical, sound-absorbing materials to enable reliable detection. The process values related to the material are read out, and the switching thresholds set accordingly. For mounting, the housing of the transmitter and the corresponding receiver can also be selected according to the installation situation. It is also possible to combine the cubic receiver (U500) with the cylindrical transmitter (UR18). The choice of sensor housing and a variably adjustable detection range thus offer great flexibility in the design-in.
​​​​​​​
In addition, as with all other variants of the U300 as well as U500/ UR18 sensor families, many other IO-Link parameters can be used by the through beam sensor in order to optimally adjust the sensor to the requirements of the application. This enables an even more reliable application solution. The sensors provide additional added value through secondary diagnostic and process data. As a result, the system effectiveness can be additionally increased and the processes can be sustainably optimized.
 

Press download


Further information

To the top