International int English

What engineers want to know using the Baumer Sensor Suite

Work with all of your IO-Link sensors in the award winning Baumer Sensor Suite.​ This free software allows you to parametrize, monitor and evaluate IO-Link devices no matter the vendor: This is the Baumer Sensor Suite.

Get started with the Baumer Sensor Suite now

How to connect any IO-Link device with only one tool?​

With the Baumer Sensor Suite you can connect to your IO-Link field masters and to engineering master devices. Establish connections to all required masters in the device cockpit. You will instantly see all sensors that are connected to the masters. You can use the dashboard for IO-Link devices of all vendors. For Baumer devices you can benefit of special add-ons to visually read sensor data.


How to handle IO-Link parameters for various applications?

The Baumer Sensor Suite helps you save device parameter sets for storage and copying. You can directly store a file from the Device Cockpit what you have just defined. You can also download the parameters set from a device and store them. Or you can define your intended parameters in the Device Library and store from there.

The Baumer Sensor Suite enables you to view and manage your parameter sets in the Device Library. As a parameter set is a standard file, you can integrate it to any application documentation workflow smoothly. You could for example bundle it to a zip for a defined release state or handle it in a version management software like GitHub.


How to stay on top of the situation when a machine fails?

The Baumer Sensor Suite allows fastest access to most IO-Link Masters and thus to connected sensors. You get up-to date sensor data: process data, type information and parameters. ​
With this information at hand, you can analyze the cause of any misbehavior. You will be able to get the application up and running easily.​
Did you know? If you are using IO-Link devices without an IO-Link Master in the application, you can connect them with our USB-C IO-Link Master and get your insights in the Baumer Sensor Suite. But to do so, you will have to disconnect the sensor from your application.​
Prepare for the undesired situation now, by experiencing the Baumer Sensor Suite now


How to get the measured value of an IO-Link sensor quickly?

The Baumer Sensor Suite makes it very easy to connect to an IO-Link Master. It supports DCP for PROFINET Masters or access via IP address for all supported IO-Link Masters. If your sensor is not connected to an IO-Link Master you can use Baumer’s USB-C IO-Link Master to get fast and direct access to your sensor.​
As you have connected the Master to the Baumer Sensor Suite, the software will directly show up sensors that are connected to the master.​
From there you can use different views to read your sensors data.​

  • Table view with all data and all details​
  • Dashboard where you can customize and select your required view​
  • Addon with predefined data analysis for Baumer products


How to install and register Baumer Sensor Suite

Are you interested to learn more about our IO-Link portfolio?

Learn more about the Baumer Sensor Suite

  • Evaluate IO-Link devices

    Understand functionality and capability through visualization

  • Precise parametrization

    Direct visual feedback of your sensor parametrization

  • IO-Link device testing

    Selecting the right sensor for your automation solution


You may also be interested in

To the top