How does a laser distance sensor work?

A laser distance sensor, also known as a laser displacement sensor, measures distances to detect objects within a certain measurement range. Laser distance measurement sensors may be based on a variety of technologies. One of the most important ones is the triangulation principle. Here, a laser point or a laser line is projected onto the object whose position needs to be determined. The object reflects part of the incident light, which is in turn detected by a receiving element within the sensor. The position of the reflected light on that receiving element depends on the distance between the sensor and the object. Hence, when the distance changes, so does the position of the signal on the receiving element. With proper calibration, the sensor can measure the object's distance with high precision.

Find out more about laser distance sensors:


Laser triangulation

Triangulation is a geometric method used to measure distances by forming a triangle between known reference points and the target object. The key element is a laser source which emits a beam of light toward a target. The light reflects off the target and is captured by a receiving element which is sensitive to the position of the signal. The angle of incidence changes as a function of object distance, and hence, the position of the signal on the receiving element changes accordingly. Using pre-calibrated data, it is then possible to extract the distance between sensor and object, based on the position of the signal on the receiver.  

With ever-improving performance of the critical components, the measurement performance of the sensors improves as well, in particular on very challenging surfaces. Examples include very smooth, shiny surfaces which result in a very low signal on the receiving element.  
Triangulation has long been a well-established technology, and still represents a very precise and reliable method for distance measurement. It is especially advantageous for measuring distances ranging from tens of millimeters to a few meters. Beyond that, other technologies are preferred, as precision and reliability using triangulation are reduced at very large distances.

Modern triangulation-based sensors offer a variety of interfaces which often allow easy, seamless integration into the control system. IO-Link is ubiquitous, as are other serial-based interfaces. Higher-end products also offer Ethernet-based protocols like Profinet, EtherNet/IP, EtherCAT or OPC UA.


Measuring functions


Beam shapes

Besides different dimensions and ranges also beam shapes are an important factor. Thanks to continuous further development,
Baumer can offers three different beam forms in its portfolio:
Discover our products:

Characteristics of laser distance sensors


Time-of-Flight (Run time measurement)

With the time-of-flight measurement method distances are measured indirectly by measuring the time required by a signal to travel the length of the range to be covered. This translates into the real world as follows: a sender unit is emitting a burst signal which, when reflected by an object, is picked up by the sensor's receiver. The sensor's electronics evaluates the time elapsed and/or the phase-shift encountered which is then converted into distance information. By applying the run time technology objects can be detected precisely and reliably even at long distances.

To the products

To the top