When attaching the magnet make sure that its magnetization direction (north / south pole) is aligned in a parallel manner to the sensor’s sensing face. The carrier material to hold the magnet should be non-ferromagnetic (e.g. no steel), otherwise it will hamper the sensing distance.
Working distance
The magnet rotor or the permanent magnet must be attached within the specified working distance to the sensor. Observe the specifications in the data sheet for axial displacement.
For coarse zero signal tuning, align the keyways provided at sensor and magnet rotor (accessory) with each other. Finetuning will be performed electronically by the downstream control. Clockwise rotation of the permanent magnet will generate a rise in the output signal.