How does a pressure sensor work?

A pressure sensor is essential for accurate pressure measurement. Baumer pressure sensors are based on resistive and piezoresistive pressure measurement. Changes in electrical resistance are measured and converted into an electrical signal. The basis for this is a metal, ceramic or piezoresistive material whose electrical resistance changes depending on the pressure acting on the material.

Pressure measurement is one of the most important and widely used technologies for monitoring and controlling machines and systems in process technology. Baumer offers a comprehensive portfolio of pressure sensors for a wide range of applications.

To the products

Absolute, relative & differential pressure

Absolute:

Relative:

Compound:

Differential:

Diagram illustrating the different pressure types

Structure and types of pressure sensors

Baumer pressure sensors basically work with two different pressure measurement methods. The method to be used depends on the intended use of the sensor.

Resistive pressure measurement:
In resistive pressure measurement, the deformation of a thin metal body or a ceramic membrane leads to a change in electrical resistance. When the metal strip is stretched by pressure, it becomes longer and its electrical resistance increases. When the metal strip is compressed, its cross-sectional area increases and its electrical resistance decreases. The change in resistance is then recorded as an electrical signal and converted into pressure.

Piezoresistive pressure measurement:
This principle is also based on the change in electrical resistance when a material is deformed. However, this measurement principle uses a piezoresistive material. This material has the property that the mechanical stress that occurs during deformation (stretching or compression) also causes a change in electrical conductivity. The change in resistance is greater than with resistive pressure measurement.

In addition to the types of pressure measurement and pressure sensors listed here, piezoelectric, capacitive and inductive pressure sensors are also mentioned, as well as vacuum pressure sensors, frequency analogue pressure sensors and pressure sensors with Hall element.

Contact us

Pressure sensor technology


Suitability for gas applications

Table with a clear overview of the suitability of Baumer pressure sensors for gas applications

Pressure in sterilization processes

Hot steam is used to sterilize devices and equipment. Small elements, such as sensors (PBMH autoclavable), can be sterilized in a suitable chamber (autoclave). In larger installations, hot steam is fed through the system, which is described as “Sterilization in place” (SIP). Accordingly, a sensor must be designed to be robust, although the signal is generally not transmitted during the sterilization process. It must survive the prevailing temperature and pressure for the relevant time span (e.g., 134 °C at more than 3 bar for 30 min). In physical terms, pressure and temperature are coupled directly with each other, which is shown in the saturated steam curve.

Diagram showing the saturated steam curve - pressure of saturated steam depending on the temperature
Pressure of saturated steam with respect to temperature

Baumer PBMx and PFMx pressure sensors are ideal for controlling the sterilization process. They provide accurate values even in the event of fast changes in temperature, and thus control the process reliably by monitoring pressure, which leads to the corresponding temperature.

Diagram showing the measuring range, overpressure range and destructive range
Definition of the pressure ranges

Explanation of terminology and relationships

Graphic illustrating the definition of sensor precision
  • Precision: This describes the possible deviation of a single measurement from the average of many measurements and can be interpreted as a dispersion circle. High precision: small dispersion circle, low precision: large dispersion circle.
  • Accuracy: This describes the distance (offset) of the average value of many measurements from the true value. High accuracy: small offset, low accuracy: large offset.
  • Standard error of measurement: This information is obtained through the best fit straight line, BFSL, and describes precision (dispersion circle).
  • Maximum error of measurement: This contains the standard error of measurement and the offset of a sensor.

Temperature dependence

The application may deviate from the reference temperature (e.g. 20 °C), so that the standard or the maximum error of measurement must be regarded in a differentiated manner.

Temperature dependence of the maximum error of measurement
Diagram showing temperature dependence in relation to measurement error

In many cases, a temperature-stable sensor with lower initial accuracy is to be preferred to a more unstable sensor with higher initial accuracy if the operating temperature deviates from the reference temperature (e.g. 20 °C).

Error indication

Baumer specifies the “maximum error indication”, i. e. statistically, 99.7% of the sensors comply with the specification. Some competitors enter the “typical error indication”, in which 32% of the products do not comply with the specification.

Diagram of error indication and percentage of sensors complying with specifications

Unit Conversions

Conversion table of the different pressure units

You may also be interested in

To the top