Part of the Baumer GAPI SDK is the so called runtime which is required to build a custom application. It provides all necessary components to integrate a Baumer camera and control it via C++ or C#.
On a development system the Baumer GAPI is usually installed using the Windows® installer or the Linux® package-manager.
The installation does:
Notice |
The installation of the Baumer GAPI with the installer/packet-manager is not necessary for the deployment of a Baumer GAPI vision application. All necessary steps can be done manually or integrated into your usual deployment process. |
The Baumer GAPI Programmers Guide explains how to create an application for the Windows® or Linux® operating system. The Programmers Guide also explains which headers and libraries need to be linked and copied to the target system.
Notice |
If no USB cameras are used, the USB producer (bgapi2_usb.cti) and its configuration (bsysusb.xml) can be omitted. |
On a Linux® System no additional drivers are required as the standard USB driver (libusb) is used.
To use Baumer USB cameras on a Windows® system it is necessary to install the included USB driver. The driver is located in the directory <InstallDir>/driver/. You will find drivers for Windows® 7 and 10, each for x64 und x86.
On Windows® systems it is beneficial to use the provided GigE filter driver. This driver helps to efficiently handle the data-stream of GigE cameras and therefore reduces the system-load. The GigE filter driver can be found in the directory <InstallDir>/driver/. You will find drivers for Windows® 7 and 10 each for x64 und x86.
The driver installation can be done in a «silent-mode». This helps with integration into custom setups or deployment-processes. You can learn more about the supported command-line parameters by starting the installer with the parameter bdriver_usb64.msi /? or bdrivermanager.exe /? .
Notice |
Windows® 7 systems without Service Pack 1 Because of security requirements of Windows® 10 it is no longer possible to install the Baumer GAPI and it’s drivers on an unpatched Windows® 7. However with some limitations it is possible to deploy an Baumer GAPI vision application on such a system. You will need an development system on which the Baumer GAPI can be installed (min. Windows® 7 with Service Pack 1). A release version of your application can be compiled here and manually copied on the target system. |
Limitations:
Please contact our Technical & Application Support Center with any questions.
Phone: +49 3528 4386 845
E-mail: [email protected]